Technical FAQs

Ask a Question

What should be remembered in the product selector about lineside and loadside connections and sections adjacent to each other?

Always be sure that sections adjacent to each other refer to each other by the correct name. This way the selector knows which sections must remain adjacent to each other. For example: A main switch next to a cold sequence meter section should have ``cold sequence meter section`` as the loadside connection. An error message will appear requesting this information.


CTA-ID : 2015247
Was this helpful?
What can we do to improve the information ?