Technical FAQs

Ask a Question

What is the maximum ambient temperature rating for 9037EG float switch?

Temperature limitations for all float switches:
Ambient Min. -30 degree C (-22F)
Max 104 degree C ( 220 F)


CTA-ID : 2015055
Was this helpful?
What can we do to improve the information ?