Technical FAQs

Ask a Question

What is the current rating of a 9080 Type G terminal block jumper?

The current rating is equal to the highest rating of the terminals the jumper was designed for. Example: a 9080GH73 jumper is designed for use with 9080GK6 40 amp or 9080GR6 60 amp terminal blocks. The maximum current rating is 60 amps.

CTA-ID : 2014865
Was this helpful?
What can we do to improve the information ?