Technical FAQs

Ask a Question

What is the ordering code for the 883958M NEMA 12?

Option code ``A`` should be placed in the 3rd location of the part # build after the hp rating for Enclosure Type 12.

To obtain Nema type 1 would place a ``G`` in this location and for Type 1G would input ``B` into this location.


CTA-ID : 2014858
Was this helpful?
What can we do to improve the information ?