Technical FAQs

Ask a Question

Is the Whole House Surge Breaker Plus suitable for use on a power system using the X10 protocol for switching loads?

The Whole House Breaker Plus is compatable on a power line using the X10 protocol.

CTA-ID : 2014857
Was this helpful?
What can we do to improve the information ?