Technical FAQs

Ask a Question

Please clarify what is meant by 1.2W standard to 3.0W maximum regarding the possible burden of the 8501KUD relay?

This is the tolerance that is possble. 1.2W is more common but it can be as high as 3W


CTA-ID : 2015245
Was this helpful?
What can we do to improve the information ?