Technical FAQs

Ask a Question

Can the 115VAC single phase input ATV11 drives be used on a 115VAC single phase motor?

No, the 115VAC single phase input ATV11 is a 230VAC three phase output drive.


CTA-ID : 2015241
Was this helpful?
What can we do to improve the information ?