Technical FAQs

Ask a Question

Can I put more than one wire in each hole of an LBA power distribution block? I want to use an LBA362104, which has a capacity of 4 wires on the output side, but I need to land more wires than 4.

No. Per Rick Potter in Raleigh, it is not advisable to do so because of torque requirements.

CTA-ID : 2015008
Was this helpful?
What can we do to improve the information ?