Technical FAQs

Ask a Question

To use the 9999SA2 kit with the NEMA starter, is the 999BLX bracket also needed?

No. The 9999SA2 comes with its own bracket to allow it to be mounted to the front of the starter.

CTA-ID : 2015228
Was this helpful?
What can we do to improve the information ?