Technical FAQs

Ask a Question

Customer has a EZML334225 and wants to know if the meter sockets are all Class 320 Sockets installed in the device?

YES, ALL of the EZML3..... devices have Class 320 meter sockets.


CTA-ID : 2015226
Was this helpful?
What can we do to improve the information ?