Technical FAQs

Ask a Question

What must be done in order to select fuses for a switch in the Medium Voltage Metal Enclosed Product Selector?

Select ``Integrated (Device + Fuse)`` on the General Application Screen for the equipment short circuit bracing question. If ``Fully Rated`` is picked then fuses cannot be chosen or used.

CTA-ID : 2015051
Was this helpful?
What can we do to improve the information ?