Technical FAQs

Ask a Question

How much mounting space does an RGA, RJA or RLA I-Line breaker use?

An R frame breaker uses 15`` of mounting space. The ``A`` in RGA, RJA and RLA indicates it is an I-Line style breaker. All the I-Line versions are 100% rated.

CTA-ID : 2014829
Was this helpful?
What can we do to improve the information ?