Technical FAQs

Ask a Question

What are the dimensions for the 450hp and 500hp 8839 58M unit?

The total width is 25 in (635mm), total height is 91.50 in (2324.1mm) and depth is 20.00 in (508mm).
The weight of the unit is 975lbs (442.2 kg).

These are the dimensions for all Enclosure size J units which include 300-500hp VT units @ 460v.

CTA-ID : 2014828
Was this helpful?
What can we do to improve the information ?