Technical FAQs

Ask a Question

Will the 9422 Type R flange mounted rod operated variable depth operating mechanisms accept the FCL, KCL, LCL circuit breakers?

No, these circuit breaker operating mechanism are not designed or UL approved for use with these high interrupting circuit breakers.


CTA-ID : 2014986
Was this helpful?
What can we do to improve the information ?