Technical FAQs

Ask a Question

What are the replacement parts for the H361A, series F6? (may be shown as F06)

The replacement parts for the H361A, series F6 (F06) are as follows. No other parts are available.

Line Base Assembly - 4056642050 (requires one per switch. Arc suppressor assembly, fuse puller not included)
Load Base Assembly - 4056002550K (requires one per switch)
Arc Suppressor Assembly - 4056669451 (requires one per switch)
Fuse Puller Kit - FPK03
Lug Assembly - 4025101652 (per lug)
Switch Mechanism - 4056610750 (recommend replacing switch mechanism gasket)
Switch Mechanism Gasket - 4056665601
Handle Assembly - 4056684150K
Handle Gasket - 4056603101
Lockplate - 4056637601
Line & Load base mounting screw - 4020516001 (3 for line & 2 for load)
Arc Suppressor mounting screw - 4020514501 (1 required)
Lockplate mounting screw - 2299940562 (2 required)
Equipment Ground Lug Kit - GTK03


CTA-ID : 2014823
Was this helpful?
What can we do to improve the information ?