Technical FAQs

Ask a Question

Are electrically interlocks available for 92345?

Yes, an electrical interlock is available as a factory-installed accessory. For one NO/NC contact, add EI suffix to the catalog number of the switch. For two NO/NC contacts, add EI2 suffix to the catalog number of the switch.


CTA-ID : 2014979
Was this helpful?
What can we do to improve the information ?