Technical FAQs

Ask a Question

What are the repair parts for the H224A, series F6? (may be shown as F06)

The list of repair parts is needed for Safety Switch catalog number H224A, series F6.

Product Line:
Heavy Duty Safety Switch

Applicable only to H224A, Series F6

The repair parts numbers for the H224A, series F6, are shown in the below list. These are the parts that can be replaced. Other parts are not replaceable.

The replacement parts for the H224A, series F6 (F06) are as follows. No other parts (enclosure, labels) are available.
-Complete Line Base - 4056702950 (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Line Base mounting screws - 4020546401 (requires 6 per line base)
-Load Base Assembly - 4056677450 (requires one per phase - includes phynolic base, lugs and fuse clips)
-Load Base mounting screws - 4020546401 (requires 2 per load base)
-Arc Suppressor Assembly - 4053922001(requires one per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056678650 (also requires Interlock Shaft Gasket 4056786001)
-Switch Mechanism mounting screws- 2299940562 (requires 2)
-Handle Assembly - 4056663550 (requires handle gasket 4056603101)
-Lockplate - 4056672101
-Lockplate mounting screws - 2299940562 (requires 2)
Was this helpful?
What can we do to improve the information ?