Technical FAQs

Ask a Question

XCKP2102G11: What are the min and max contact block screw torque values.

Contact block XES..P
Min torque 7.1 lb-in
Max torque 10.6 lb-in


CTA-ID : 2014817
Was this helpful?
What can we do to improve the information ?