Technical FAQs

Ask a Question

Customer is looking at the potentiometer type 9001SK. What is the dimension of the dial plate?<br /><br />

9001K20................9001 KN905 1.719 inches square
9001SK20.............9001KN180WP is 2.210 inches square




CTA-ID : 2014797
Was this helpful?
What can we do to improve the information ?