Technical FAQs

Ask a Question

Is gold flashed contacts an option on NT breakers? If so is there a part number and how would it affect the breaker part number? Is this in the beaker product selector? How does this affect the actual cost of the breaker?

There are gold flash contacts for the NT only, not the NW. The standard NW OF contacts have a 24V, 10mA minimum.
The NT contacts are selectable on the NT. Character A in position 11. See pricing guide for pricing info.


CTA-ID : 2014791
Was this helpful?
What can we do to improve the information ?