Technical FAQs

Ask a Question

Customer has a 9001OR120 and needs to know if the Colored Lens can be replaced ?

Issue:
Customer has a 9001OR120 and needs to know if the colored lens can be replaced ?
Product Line:
Compact Pilot Lights       
Environment:
9001 Type O, Nema 13 Pilot Lights
Cause:
Lens are being requested to be changed to a different color without changing the entire part out.
Resolution:
Yes part number is 2550420020

Color Catalog Number
Red .......2550420020
Green ....2550420040
Amber.... 2550420060
Clear ......2550420010
Yellow.... 2550420030
White .....2550430040   
Blue .......2550470010


CTA-ID : 2014790
Was this helpful?
What can we do to improve the information ?