Technical FAQs

Ask a Question

Can a NEMA replacement melting alloy overload relay for a Square D starter be converted to one that is suitable for separate mounting?

Product Line:
 
NEMA style Overload Relays

Resolution:
 
No, lugs cannot be added to the bus stabs nor are the stabs removable.


CTA-ID : 2015177
Was this helpful?
What can we do to improve the information ?