Technical FAQs

Ask a Question

What are the replacement parts for the H362A, series F6? (may be shown as F06)

Issue:
Repair Parts

Product Line:
HD SS

Cause:
Maintenance

Resolution:
The replacement parts for the H362A, series F6 (F06) are as follows. No other parts are available.

Line Base Assembly - 40566-038-50 (requires one per switch. Arc suppressor assembly, fuse puller not included)
Load Base Assembly - 40566-040-50 (requires one per switch)
Arc Suppressor Assembly - 40566-355-50 (requires one per switch)
Fuse Puller Kit - FPK0610
Lug Assembly - 40251-016-52 (per lug)
Switch Mechanism - 40566-469-50 (recommend replacing switch mechanism gasket)
Switch Mechanism Gasket - 40566-032-01
Handle Assembly - 40566-635-50
Handle Gasket - 40566-031-01
Lockplate - 40566-721-01
Line & Load base mounting screw - 40205-151-01 (3 for line & 2 for load)
Arc Suppressor mounting screw - 40205-145-01 (1 required)
Lockplate mounting screw - 22999-405-62 (2 required)
Equipment Ground Lug Kit - GTK0610



CTA-ID : 2014955
Was this helpful?
What can we do to improve the information ?