Technical FAQs

Ask a Question

What are the repair parts for the H324A, series F6? (may be shown as F06)

Product Line:
Heavy Duty Safety Switch

Applicable only to H324A, Series F6

The repair parts numbers for the H324A, series F6, are shown in the below list. These are the parts that can be replaced. Other parts are not replaceable.

The replacement parts for the H324A, series F6 (F06) are as follows. No other parts (enclosure, labels) are available.
-Line Base Assembly - 4056703050 (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Load Base Assembly - 4056677450 (requires one per phase)
-Line & Load base mounting screw - 4020546401 (6 for line base & 2 for load base)
-Arc Suppressor Assembly - 4053922001 (requires one per phase)
-Lug Assembly - 4025116251 (per lug)
-Switch Mechanism - 4056678650 (recommend replacing switch mechanism gasket 4056786001)
-Handle Assembly - 4056663550 (recommend replacing handle gasket 4056603101)
-Lockplate - 4056672101
-Arc Suppressor mounting screw - 4020514501 (1 required per phase)
-Lockplate mounting screw - 2299940562 (2 required)
-Equipment Ground Lug Kit - PKOGTA2
Was this helpful?
What can we do to improve the information ?