Technical FAQs

Ask a Question

Is there an optional lug kit for an NF442L2 to accept (2) 3/0kcmil wires?

Yes. Use an NOALM2 kit. Per Digest 173 page 8-15 footnote, it will require an additional 6 inches to the box height. A larger enclosure will be required. The NOALM2 kit contains the rail and deadfront extensions necessary to install the interior in the larger enclosure.

Revised 4/29/04

CTA-ID : 2014760
Was this helpful?
What can we do to improve the information ?