Technical FAQs

Ask a Question

What is the lug wire range for QH or QHB breaker?

Wire range is (1 or 2) #14-10 copper or (1) - #14-8 per phase aluminum or copper.


CTA-ID : 2014948
Was this helpful?
What can we do to improve the information ?