Technical FAQs

Ask a Question

What are the replacement parts for the H223A, series F6? (may be shown as F06)

The replacement parts for the H223A, series F6 (F06) are as follows. No other parts are available.

Line Base Assembly - 4056775350 (requires one per switch. Arc suppressor assembly, fuse puller not included)
Load Base Assembly - 4056609550 (requires one per switch)
Arc Suppressor Assembly - 4056635550 (requires one per switch)
Fuse Puller Kit - FPK0610
Lug Assembly - 4025101851 (per lug)
Switch Mechanism - 4056646950 (recommend replacing switch mechanism gasket)
Switch Mechanism Gasket - 4056603201
Handle Assembly - 4056663550
Handle Gasket - 4056603101
Lockplate - 4056672101
Line & Load base mounting screw - 4020515101 (3 for line & 2 for load)
Arc Suppressor mounting screw - 4020514501 (1 required)
Lockplate mounting screw - 2299940562 (2 required)
Equipment Ground Lug Kit - GTK0610





CTA-ID : 2014937
Was this helpful?
What can we do to improve the information ?