Technical FAQs

Ask a Question

What is the mean time between failure for the ATV11 unit?

The MTTF ( MTBF ) of ATV11 is 200,000 hours for an ambient temperature 30*C.


CTA-ID : 2015352
Was this helpful?
What can we do to improve the information ?