Technical FAQs

Ask a Question

What is the recommended fuse part number for ATV58HD79N4XZU?

There are fuse and circuit breaker recommendations in the attached document. The recommendations are the maximum allowable sizes. Lower fuse ratings may be used according to electrical codes. Consideration should be made for proper cable size and overcurrent protection.

For Constant Torque Low Noise 60 HP, Fast-acting Class J fuses 200 A Class T fuses are acceptable.
For Constant Torque or Variable Torque Low Noise 75 HP, Fast-acting Class J fuses 175 A. Class T fuses are acceptable.
For Variable Torque 100 HP, Fast-acting Class J fuses 200A. Class T fuses are acceptable.


CTA-ID : 2015344
Was this helpful?
What can we do to improve the information ?