Technical FAQs

Ask a Question

How do I find HELP/Information about the Question on the screen ( Left column ) in the Medium Voltage Metal Enclosed Product Selector?

Click on the button with the Arrow and Question Mark on it. This button is on the toolbar. A question mark will attach to your cursor. Move the cursor to the item in question and click once on that item. This will open up the Help Screen for that item. You can also click on HELP on the menu bar. Both of these methods will get to the same information database.

CTA-ID : 2015144
Was this helpful?
What can we do to improve the information ?