Technical FAQs

Ask a Question

What are the fuse sizes for Fuselogic Delayed Fuse Tripping with Square D fuses for HVL/cc Switchgear? (Control power required)<br />

5kV - 200E - 1080A
15kV - 150E - 480A
17.5kV - 150E - 270A
25.8kV - 80E - 180A
38.0kV - 65E - 117A



CTA-ID : 2015142
Was this helpful?
What can we do to improve the information ?