Technical FAQs

Ask a Question

What are the fuse sizes for Fuselogic Direct Fuse Tripping with Square D fuses for HVL/cc Switchgear? (No control power required)<br />

5kV - 10E - 175E
15kV - 10E - 125E
17.5kV - 10E - 125E
25.8kV - 10E - 65E
38.0kV - 10E - 50E



CTA-ID : 2015141
Was this helpful?
What can we do to improve the information ?