Technical FAQs

Ask a Question

Customer asks if the MP40H1, 4000a Masterpact breaker with the STR58UT trip unit has the option of shutting the Instantaneous trip function off?

The H1 version allows the instantaneous to be turned off.

CTA-ID : 2015136
Was this helpful?
What can we do to improve the information ?