Technical FAQs

Ask a Question

Does the rating of 104 Degrees F that the 8839 58M bulletin specifications indicate for operating temperature refer to the internal temperature of the enclosure or the air temperature of the surrounding area?

This is the ambient air temperature. This does not refer to the internal enclosure temperature.

CTA-ID : 2015137
Was this helpful?
What can we do to improve the information ?