Technical FAQs

Ask a Question

Can a factory-installed provision for a keylock be ordered with an NT cradle?

We do not offer the selection of provision only for a cradle key interlock. The provision consists of a plate, mounting screws, lock actuator cams and screws. If we provided the provision only, we could install the plate but would have no place to install the lock actuator cams which must be installed on the key lock.

CTA-ID : 2015135
Was this helpful?
What can we do to improve the information ?