Technical FAQs

Ask a Question

Do the General Duty Safety Switches have copper or aluminum lugs?

Issue:
Product design features

Product Line:
General Duty Safety Switches

Environment;
Main Lug material

Cause:
Application

Resolution:
General Duty Safety Switches have aluminum lugs as standard, which accept both copper and aluminum wire. There are no optional copper lugs available.

 
Was this helpful?
What can we do to improve the information ?