Technical FAQs

Ask a Question

Is a low pressure cutoff option available on the 9012GNG5?

No it is not. Use either 9012G machine tool switch with lock on falling pressure or a 9013FSG with low pressure cut out.


CTA-ID : 2015332
Was this helpful?
What can we do to improve the information ?