Technical FAQs

Ask a Question

Do the Altivar drives meet the IEEE C62.41 standard?

Our 230 volt rated drives meet that standard for Location Category B1.
Our 460 volt rated drives meet that standard for Location Category B2.
This is true for ATV58, ATV66, ATV61, ATV71 & ATV31 drives.


CTA-ID : 2015127
Was this helpful?
What can we do to improve the information ?