Technical FAQs

Ask a Question

Does the H800SNE4 solid neutral assembly used with the Square D 800amp Heavy Duty Safety Switches, come with a bonding strap?

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Environment:
Accessories

Cause:
Application

Resolution
Yes, this solid neutral assembly will come with the appropriate bonding means for bonding the switch in the field for use in Service Entrance Applications.




CTA-ID : 2015324
Was this helpful?
What can we do to improve the information ?