Technical FAQs

Ask a Question

What are the torque specs for the Main Lug Wire binding Screws on a H323AWK?

The torque specs are as follows:
#10 - 14 = 35 in-lbs
#8 = 40 in-lbs
#4-6 = 45 in-lbs
#1/0 - 3 = 50 in-lbs


CTA-ID : 2015318
Was this helpful?
What can we do to improve the information ?