Technical FAQs

Ask a Question

On a 8501KU style relay what amperage ratings does it have when used on 120vac

15 amps continous with a resistive 75% pf
3 pole devices have a 30 Amp max. total (sum of currents in all 3 poles), continuous rating.

CTA-ID : 2015109
Was this helpful?
What can we do to improve the information ?