Technical FAQs

Ask a Question

What are the dimensions and weight of the ATV58HD16M2XZU, ATV58HD23M2XZU, ATV58HD28N4XZU, ATV58HD33N4XZU, and ATV58HD46N4XZU drive?

The dimensions are 9.45 inches (240 mm) (W), 21.65 inches (550 mm) (H), and 11.14 inches (283 mm) (D) .

The weight is 75 lb (34 kg).

These values are the same for all size 6 frame size ATV58 which include:
...D16M2, D23M2, D28N4, D33N4 & D46N4

CTA-ID : 2015108
Was this helpful?
What can we do to improve the information ?