Technical FAQs

Ask a Question

Why don`t we offer the selection of provision only for a cradle key interlock?

The provision consists of a plate, mounting screws, lock actuator cams and screws. If we provided the provision only, we could install the plate but would have no place to install the lock actuator cams which must be installed on the key lock. When the customer wanted to install the key lock, they would have to remove the plate anyway so we decided to only supply the provision as a kit. It is really easier for the customer and there is less chance of losing small parts.

CTA-ID : 2015104
Was this helpful?
What can we do to improve the information ?