Technical FAQs

Ask a Question

What is the torque for the ``bolted bus connection`` for the load side of the main breaker (QB, QD, QG, QJ) for the QO three phase load center (ex. QO342MQ225)?

Breaker wire binding screws 100-250 in./lbs and the bus conectors to the interior 50-90 in./lbs.


CTA-ID : 2015103
Was this helpful?
What can we do to improve the information ?