Technical FAQs

Ask a Question

What is the replacement bus fingers for a QON442MS400 QO load center

Issue:
Repair Parts

Product Line: 
Obsolete QO LC

Cause:
Maintenance

Resolution:
B phase is 80110-601-02 , A and C phases are 80110-600-02, screws are 80110-802-01


CTA-ID : 2015043
Was this helpful?
What can we do to improve the information ?