Technical FAQs

Ask a Question

Can I get the height of metal ring nuts used on 9001 type operators? Dimensions on page 159 of the specifiers guide are confusing.

The full guard is 9/16`` and the extended guard is 11/16``. The no guard is 1/4``.

CTA-ID : 2014910
Was this helpful?
What can we do to improve the information ?