Technical FAQs

Ask a Question

What is option J09 on a Econoflex

This option provides a controller interface for a 0-10 VDC customer-supplied auto speed reference signal into the AI2 input using a 0-10 V/4-20 mA converter with a 40 kOhm impedance.

This input can be used as the speed reference 2 signal for Automatic mode speed reference.

CTA-ID : 2015101
Was this helpful?
What can we do to improve the information ?