Technical FAQs

Ask a Question

What are the dimensions for 8639 LPA4NA & LNA4NA?

Issue: What are the dimensions for 8639 LPA4NA & LNA4NA?
 
Product Line: 8639 ATS46
 
Environment: 8639 LPA4NA & LNA4NA
 
Cause: N/A
 
Resolution: Theses are Floor mount unit at 34.21 inches wide, 92.68 inches tall, 26.00 inches deep with disconnect handle extended.

The wieght is 850 lbs

This is the same for class 8638 & 8639 Type NI - NQ standard duty and LM - LP heavy duty.


 
Was this helpful?
What can we do to improve the information ?