Technical FAQs

Ask a Question

Do we have any enclosed products with Seismic rating?

Yes. THe 8839 58M Floor Mounted Enclosure product has a Seismic Certification when the H10 Option is selected when order is buildt.

It provides a certification label and hardware certified to seismic rating AC156 harmonized with NFPA 5000 and IBC 2000 standards.

This information can be located in the 30072-450-71 bulletin.

CTA-ID : 2015087
Was this helpful?
What can we do to improve the information ?