Technical FAQs

Ask a Question

Is there a HOM160 Homeline breaker?

No, the maximum Homeline single pole breaker is 50 A. QO160 1 pole 60A available with QO breaker


CTA-ID : 2014465
Was this helpful?
What can we do to improve the information ?